Example Programs and Installation Folders
Example Programs
Most example programs listed in this help, as well as many other code samples, are available at http://www.keysight.com/find/iosuite. Code examples are only for Windows at this time.
IO Libraries Suite Installation Folders
See the appropriate section below for Windows
or Linux.
Windows
Click the Keysight IO Control
and select About Keysight IO Libraries Suite to see the specific installation directories used on your PC, as shown below.
Linux
In Linux, IO Libraries suite is installed at: /opt/keysight/iolibs